• Default Alternative Text

    Defence

    Schneider Electric make many of the systems and technology that make many of the Defence Estate work.

Default Alternative Text

Challenges

The Defence Estates are truly unique. No one else has such a large disparate estate made up of everything from ports to hospitals, which brings unique challenges that are compounded by an ever increasing need to reduce costs and become more efficient. With such complex challenges as these, you need the specialist expertise of an organisation that has over 50 years experience in working with the MoD.

Why work with Schneider Electric

  • Default Alternative Text Secured technology Our technology sits in boxes and rooms all over the estate, you will have seen them, they’re the ones usually labelled ‘Keep Out’ or ‘Authorised Persons Only’.
  • Default Alternative Text Safe electricity Quietly and efficiently our technology distributes and controls electricity around defence sites, whether it’s a security system or a light, you can be sure it’s safe, reliable and green.