• Default Alternative Text

    Start-Up and Commissioning Services

    Minimize costly downtime from the start

An employee checking on the electrical machine and writing down what he notices, energy management, power management, field service

Challenges

Improper installation is a leading cause of equipment failure.
Having improper equipment installation can cause costly downtime and delays. At Schneider Electric, our goal is to keep your business up and running as efficiently as possible.
  • Solutions

    Our Start-up and Commissioning solution includes:
    • Confirm the system has been installed properly
    • Confirm the equipment operates as specified
    • Identify and notify the owner of equipment modifications that may be required
    • Gather and evaluate initial operational data
    • Verify correct operation of all interfaces between new and existing equipment
  • Value Proposition

    Our goal is to confirm your equipment is installed properly, meets factory standards and passes our stringent performance tests so you can minimize downtime delays in the future.
  • Differentiation

    We visually, electrically and mechanically inspect equipment to make sure it is in compliance with purchase specifications and design intent and that no damage occurred during shipment. We check the equipment and all of its components such as PLCs, protective devices, relays and timers to make sure they are set up properly and functioning correctly. Beyond that, we perform electrical testing to check insulation, current path, functionality, sequencing and more.
Default Alternative Text

Explore More Solutions To Help Optimize Your New Investment

Schneider Electric Services is here to help maximize your investment throughout the entire product life cycle.

Benefits

  • A man recording his findings from an electrical box, sustainability reporting, electric utilities, electric power distribution.

    We provide start-up and commissioning on any brand of equipment
    NFPA 70B section 31.5 specifically cites “Square D Services” testing procedures to be acceptable along with NETA and manufacturer testing specification
  • Default Alternative Text

    Confirmation that equipment is installed and functioning according to specifications
    Simple and immediate warranty resolution
  • Default Alternative Text

    Qualified technicians, knowledgeable in the latest design specifications and product developments
    On-site assistance with the integration of products on complex projects
  • Default Alternative Text

    Additional six months of extended warranty coverage on drives.
    National network of service locations and qualified experts, available 24/7.