• Default Alternative Text
    Improve Power System Reliability and Lower Life Cycle Costs

    Switchgear Modernization Solutions

Default Alternative Text

Challenges

Repair? Replace? Modernize!
When considering whether to repair or replace existing switchgear, there are a number of factors to consider. These may include the operating environment, availability of spare parts, the impact of downtime, as well as the cost of ongoing maintenance. There may also be the need to upgrade to current technology. A viable, cost-effective strategy is to modernize the existing equipment with the latest state of the art circuit breaker solutions from Schneider Electric.
  • Solutions

    Our modernization solutions, available for any manufacturer's low- and medium-voltage switchgear, will expand the capabilities of your electrical system with minimal downtime.

    Direct Replacement circuit breakers are designed to fit into the existing cubicle with little-to-no downtime since there is minimal (if any) outage to the equipment bus.

    Retrofill Solutions involve modifying the internal circuit breaker cell to accept the new circuit breaker. A bus outage is required for the modifications.

  • Value Proposition

    Expand the capabilities of your electrical system with minimal downtime and at a fraction of the cost of purchasing and installing new switchgear. Direct replacement and/or retrofill solutions are available for any manufacturer’s equipment.
  • Differentiation

    Our modernization solutions utilize the upgraded technology of the Masterpact™ insulated case circuit breaker for low-voltage systems or the Magnum™ circuit breaker for medium-voltage systems. Both the Masterpact and the Magnum circuit breakers are installed, tested and commissioned by qualified field service personnel and are backed by a one-year warranty. Extended warranties are available.
Default Alternative Text

Learn More About Our Modernization and Upgrade Solutions

Two different modernization solutions provide the same end result: Improved power system reliability and lower life-cycle costs.

Benefits

  • Default Alternative Text

    Mastpact circuit breakers feature high ampere interrupting and short-time current ratings. ModbusTM communication protocol and field-installable devices.

  • Default Alternative Text

    Magnum medium-voltage circuit breakers are manufactured using totally new components including vacuum or SF6 arc interruption technology.