• What you need to make a sustainable solar investment

Default Alternative Text
With the right balance-of-system solution, a PV power plant can earn a great ROI. More than 3 GW The combined capacity of large 3-phase inverters installed worldwide by Schneider Electric.

The key to earning a healthy ROI on your utility-scale solar project

A balance-of-system solution integrates everything needed to efficiently distribute and manage locally generated solar energy, from panel DC output to the grid connection. A Schneider Electric balance-of-system solution typically includes the following:

  • PV Box: an optimized power conversion system that can be fully tailored for specific needs or deployed as a standard solution brick, reducing installation time and costs.
  • Conext Core XC grid-tie inverters: the core of the PV power conversion system, a 3-phase inverter with best-in-class peak efficiency (98.9%) and fully configurable, grid-interactive features.
  • Array Boxes: a robust string combiner box that enables the connection of multiple PV module strings while protecting and monitoring the installation.
  • Grid-tie Substations: an HV or MV substation that ties the installation to the grid in compliance with local codes and regulations.

Conext Control monitoring and control solution: a single, standardized solution that integrates process, supervision, and monitoring functions.