{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Operation and wiring of an LAD6K10*, LA6DK10* and LA6DK20* Mechanical...

Information: Operation of an LAD* Mechanical Latch Block A pulse on the contactor coil (terminals A1 & A2) causes the contactor to close. The LAD* module mechanically latches and holds the...

Do you have the dimensions for the Easy 9+ range of consumer units?

Please find attached PDF of dimensions for the Easy 9+ consumer units.

Why do the new iC60H vigi units trip slower than the old Multi9 Vigi units?

It's normal that the ref A9V02763 trips in a longer time than the old multi9 MGV630304 because it's A type vigi unit This new RCD uses "ACCU" technology which is better on...

Where to find the instructions for the PM700 Multi function Power Meter?

Please find attached the instruction sheet for the PM700 Milti Function Power Meter

EOTE language import/export

Export the language table to a tab delimited file (txt or csv) Excel, DataàFrom Text/CSV Select the Exported text file File Origin à 65001: Unicode (UTF-8), Délimiter à Tab Load button Modify...

What is the Maximum Zs earth fault loop impedance value for the TM30D trip...

For the NSX TM30D breakers at U=218.5V (This is including the Cmin Factor .95 as per BS7671 amendment 3:2015) - Zs (5s) = 0.722 ohms - Zs (0.4s) = 0.55 ohms

Are the CANALIS KU tap-off units still commercialised?

No, CANALIS KU tap-off units are no longer sold. The entire KU offer (with copper conductors), comprising power supplies, run components, fixing brackets, tap-off units, etc., was removed from the...

What position should the address selector have to connect directly to a...

To connect directly to a TSX NANO PLC with PL7-07, check that the dial on the terminal socket is set to address 0. Note: This platform is discontinued. Please get access to our digital catalog...

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our General Knowledge FAQsGeneral Knowledge

How to identify the M172 that I am using in the program?

In order to identify in our code which M172 model we are using we need to use the two (2) internal variables located in "Operators and blocks". The variables are Par_POLI (Polycarbonate...

Which is the software to program the Modicon M171O (Optimized)?

The software to program the Modicon M171O (optimized) is EcoStruxure Machine Expert HVAC. The software can be downloaded from our website:...

What is the difference between PNP and NPN when describing 3 wire...

Most industrial proximity sensors (inductive, capacitive, ultrasonic and photo electric) are solid state. The term solid state refers to the type of components used within the sensor. Solid state...

What are the differences between 380v AC, 400v AC and 415v AC Mains...

For many years, mainland Western Europe has used a mains, 3 phase, electricity supply nominally rated at 380v AC 50Hz while the UK used 415v AC 50Hz. Currently, all Western European 3 phase supplies...

What are the differences between 220VAC, 230VAC and 240VAC Mains Supplies...

For many years, mainland Western Europe has used a mains electricity supply rated at nominally 220VAC 50Hz while the UK used 240VAC 50Hz. In 1994, the European Union state members decided to proceed...

What size overload do I use with a star delta starter ?

In the majority of cases, the overload of a star delta starter is fitted below the delta contactor with wiring connections to one side of each of the motor windings. The other side of the windings...