{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Do you have the dimensions for the Easy 9+ range of consumer units?

Please find attached PDF of dimensions for the Easy 9+ consumer units.

Why do the new iC60H vigi units trip slower than the old Multi9 Vigi units?

It's normal that the ref A9V02763 trips in a longer time than the old multi9 MGV630304 because it's A type vigi unit This new RCD uses "ACCU" technology which is better on...

Where to find the instructions for the PM700 Multi function Power Meter?

Please find attached the instruction sheet for the PM700 Milti Function Power Meter

EOTE language import/export

Export the language table to a tab delimited file (txt or csv) Excel, DataàFrom Text/CSV Select the Exported text file File Origin à 65001: Unicode (UTF-8), Délimiter à Tab Load button Modify...

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our General Knowledge FAQsGeneral Knowledge

How to identify the M172 that I am using in the program?

In order to identify in our code which M172 model we are using we need to use the two (2) internal variables located in "Operators and blocks". The variables are Par_POLI (Polycarbonate...

Which is the software to program the Modicon M171O (Optimized)?

The software to program the Modicon M171O (optimized) is EcoStruxure Machine Expert HVAC. The software can be downloaded from our website:...

What is the difference between PNP and NPN when describing 3 wire...

Most industrial proximity sensors (inductive, capacitive, ultrasonic and photo electric) are solid state. The term solid state refers to the type of components used within the sensor. Solid state...

What are the differences between 380v AC, 400v AC and 415v AC Mains...

For many years, mainland Western Europe has used a mains, 3 phase, electricity supply nominally rated at 380v AC 50Hz while the UK used 415v AC 50Hz. Currently, all Western European 3 phase supplies...