Technical FAQs

Ask a Question

Can I order Canalis KN or KS IP55 generation in a special colour and what are the possible RAL colour charts?

Yes, you can order Canalis KN or KS IP55 generation in a special colour. 

Important: Only straight lengths and metal units can be painted.

For prices and delivery times, please contact Canalis tendering department on 0870 608 8 608
Was this helpful?
What can we do to improve the information ?