Technical FAQs

Ask a Question

How can I order spare end covers for the new CANALIS KS range from 100 to 1000 A, IP55?

The end cover previously sold separately for the KS range is now supplied automatically with the feed unit.

If the end cover is inadvertently thrown away with the unit's packaging, order one of the following part numbers:

    * KSA400AF1 for 100 to 400 A ratings
    * KSA1000AF1 for 500 to 1000 A ratings

These part numbers must be considered as spare parts and may not always be available from stock, please contact Canalis sales for stock availability on 0870 608 8 608
Was this helpful?
What can we do to improve the information ?