Technical FAQs

Ask a Question

Can I connect a busbar trunking system of the KBB25A type with a KBB40A?

Yes, you can connect a busbar trunking system of the KBB25A type directly to a KBB40A.
They are fully compatible, in terms of both mechanical and electrical connections.

Caution: The complete line then becomes a 25 A line.
Was this helpful?
What can we do to improve the information ?