Technical FAQs

Ask a Question

Are the CANALIS ranges type KB2-KB4 and KBB-KBA compatible?

The KB2-KB4 range are not compatible with the KBA or KBB range 

There are no transition or adaptor elements available for them.
Was this helpful?
What can we do to improve the information ?