Technical FAQs

Ask a Question

Are the CANALIS KU tap-off units still commercialised?

No, CANALIS KU tap-off units are no longer sold.

The entire KU offer (with copper conductors), comprising power supplies, run components, fixing brackets, tap-off units, etc., was removed from the catalogue in 1983 (year in which the offer was withdrawn from sale).

This offer was replaced by the KS range (with aluminium conductors), which is not compatible. There is no compatible offer.

The sale of spare parts for CANALIS KU tap-off units (compatible with the KR range) was discontinued at the end of 1999 (when the KU range was finally dropped).
Was this helpful?
What can we do to improve the information ?