Technical FAQs

Ask a Question

Do the SM6 cubicles contain asbestos?

No, there is no asbestos in the SM6 range of cubicles.
A certificate confirming the absence of asbestos is available in the extra info.
Extra info: 2006 SM6 certification of absence of asbestos.pdf (PDF, 158 K)
Was this helpful?
What can we do to improve the information ?