Technical FAQs

Ask a Question

What is the principle for marking components in the Sepam 1000+ range?

Each Sepam is supplied in its own packaging containing the base unit and two connectors:
  • 1 20-pin connector (CCA620 or CCA622
  • 1 6-pin connector (CCA626 or CCA627)
     
Other optional accessories such as modules, current or voltage connectors and cables are packaged separately.

Identification of the Sepam:

Check the two labels located on the right-hand flange of the base unit.
They specify the operating and hardware elements of the product.

Identification of accessories:

Accessories such as optional modules, current or voltage connectors and connection cables are identified by a label.
Was this helpful?
What can we do to improve the information ?