Technical FAQs

Ask a Question

How can I protect by password the settings of the Sepam series 80?

"Remote control and remote parameter setting of the Sepam series 80 can be password protected.

A first password can be used to protect remote control and a second to protect remote parameter setting.

Each communication port can use a different password.

The passwords can be set from the SFT2841 by selecting the ""Sepam Unit"" icon

(1) The SFT 2841 kit comprises:
  • The CCA 783 cable
  • The parameter setting and operating software
  • The function recovery software"
Was this helpful?
What can we do to improve the information ?