Technical FAQs

Ask a Question

How do I set the target value on an electromechanical Preset Counter?

XBKP50100D*0M
There is a button under each digit and reset button to the left of the display. Press the reset button and the button under the digit simultaneously to index a given digit to the required value.

XBKP50100U*0M
There is a button under each digit and another button to the left of these. Press the button to the left and the button under the digit simultaneously to index each digit to the required value. In this case the reset button zeros the count total.


Was this helpful?
What can we do to improve the information ?