Technical FAQs

Ask a Question

Do I need to Earth my ASi Power supply

For some units it is recommended to earth the ASi system at the power supply
  • ASIABLB300*
  • ASIABLM3024

For other units this is mandatory, this is because the unit is designed to detect Earth faults
  • ASIABLD300*

Earthing should be to the GND terminal

Note : The GND terminal is internally linked and it is therefore only necessary to connect to earth at one point.

Was this helpful?
What can we do to improve the information ?