Technical FAQs

Ask a Question

How can a fault be reset on a ASi power supply

If the fault is an Overload of Short Circuit fault then the fault light will go off when the fault has cleared on the following ranges:

  • ASIABLB300*
  • ASIABLD300*
  • ASIABLM3024 
If the fault indication appears on the ASIABLD300* power supplies

  • ASIABLD3002
  • ASIABLD3004

A fault can be reset in two ways:

  • Press the Reset Button on the front of the PSU
  • Send a reset by closing the contact on the unit, terminals +/-

Note : All faults should be cleared before resetting the unit.
Attached is an instruction sheet with the same information in a pictorial format
Was this helpful?
What can we do to improve the information ?