Technical FAQs

Ask a Question

Are the MGFA Switch Disconnector Fuses and the MGFL Switch Disconnectors suitable for use on DC systems?

The MGFA Switch Disconnector Fuses and the MGFL Switch Disconnectors are only suitable for use on AC systems.

The utilisation categories are:-
AC20A, AC21A,  AC22A, AC23B at rated current.
Was this helpful?
What can we do to improve the information ?