Technical FAQs

Ask a Question

Are the MGFS Fuse Switch Disconnectors and the MGFD Switch Disconnectors suitable for use on DC systems?

The MGFS Fuse Switch Disconnectors and the MGFD Switch Disconnectors are only suitable for use on AC systems.

The utilisation categories are:-
AC20A, AC21A,  AC22A, AC23B at rated current, AC23A for ratings up to 160A.
Was this helpful?
What can we do to improve the information ?