Technical FAQs

Ask a Question

The NSX MCCB trips as soon as it's switched on and the display indicates ENCT or STOP

If a 3 pole NSX MCCB is fitted with a Micrologic 5 or 6 trip unit the neutral conductor can be protected with an external CT.

If the neutral protection is enabled before the CT is connected the MCCB will trip. The display will either have "ENCT" or "STOP" on it.

The trip unit has a function that checks the continuity of the external CT and wiring, and if this cannot be detected the MCCB will trip.

To resolve this problem the front cover of the MMCB needs to be removed and either the CT needs to be connected, or terminals T1 & T2 need to be linked so that the MCCB can be reset. Please see attachment for further details.
 
Was this helpful?
What can we do to improve the information ?