Technical FAQs

Ask a Question

What is the default password of a SEPAM relay?

The default password is "0000". This is a 2 key password that allows the operator to access and change all data, including protection settings and Sepam parameter settings. The operator will also be able to clear/reset alarms and peak values.
Was this helpful?
What can we do to improve the information ?