Technical FAQs

Ask a Question

Is Sepam series 80 remote setting protected by a password?

Yes, Sepam series 80 remote control and remote setting can be protected by passwords.

A first password may be used to protect remote control and a second one to protect remote setting.

Different passwords can be used for each communication port.

The passwords are set up via the SFT2841 using the "Sepam unit" icon.

Was this helpful?
What can we do to improve the information ?