Technical FAQs

Ask a Question

What do the LED's on the ASi power supplies indicate

The ASi power supplies have several functions described by the diagram below
They are very useful for fault finding and checking the electrical status of the power supplied to the ASi network

The information shown is for the following Regulated Swithmode power supplies:
  • ASI ABLB3002
  • ASI ABLB3004
  • ASI ABLD3002
  • ASI ABLD3004
  • ASI ABLM3024

Was this helpful?
What can we do to improve the information ?