Technical FAQs

Ask a Question

Are the C60H and iC60H miniature circuit breakers sold in the UK UL approved?

The standard C60H and iC60H offered in the UK is not UL approved.

However, we do offer various ranges of C60 devices that comply with UL 1077 or UL 489 standards.

Choosing the correct circuit breakers complying with UL standards can be complicated. Therefore we recommend that you contact technical support on 0870 608 8 608
Was this helpful?
What can we do to improve the information ?