Technical FAQs

Ask a Question

What is the voltage output from the time clock output contact?

The output contacts on the time clocks are a "volts free" contact, which means that they do not obtain a supply from the time clock power supply.

The output contacts have to be fed separately. The terminlas are:-

IHP Clocks
Contact C1
Terminal 4 common, Live supply.
Terminal 6 energised when the clock is on. This terminal is normally connected to the load.
Terminal 2 energised when the clock is off.

Contact C2
Terminal 3 common, Live supply.
Terminal 5 energised when the clock is on. This terminal is normally connected to the load.
Terminal 1 energised when the clock is off.

IH Clocks
The contact only has two terminals 1 & 2. The supply and load can be connected to either terminal.
 
Was this helpful?
What can we do to improve the information ?