Technical FAQs

Ask a Question

How can the CT module be fitted onto NSX moulded case circuit breakers since the fixings screws on the CT module are M6 and the terminals on the NSX MCCB are M8?

The M8 terminal nut inserts on the MCCB have to be swapped with the M6 terminal nut inserts on the CT module.

Please see page 2 of the attached Instructions
Was this helpful?
What can we do to improve the information ?