Technical FAQs

Ask a Question

What is the largest RCCB Incomer for the Acti9 3 phase Distribution Board ?

The largest RCCB Incomer is 160A, and the part number is SEA9NI160RCCB.
The sensitivity is adjustable - 30mA, 300mA, 1A, 3A, and 10A
The kit comes complete with lugs, terminal shields and a 400mm high extension enclosure.
Was this helpful?
What can we do to improve the information ?