Technical FAQs

Ask a Question

Do the EGX100 and EGX300 Gateways require external power supplies?

The EGX100 and EGX300 Gateways require a 24V DC power supply. This can be supplied to the device in two ways:-
  • Power-Over-Ethernet (POE[IEEE 802.3af])
  • 24V DC auxiliary power supply

Suitable auxiliary power supplies with a 24V DC output are:-
 
Input Voltage  Part No.
24-30V DC 54440
48-60V DC 54441
125V DC 54442
110V AC 54443
220V AC 54444
380V AC 54445
 100-240V AC  ABL8MEM24003
   


See attached user guides for further information.
Was this helpful?
What can we do to improve the information ?