Technical FAQs

Ask a Question

Are the CT contactors suitable for switching DC power systems?

The CT contactors are suitable for switching 250V AC (1 & 2 pole) and 400V AC (3 & 4 pole) Utilization Category AC7a

They are not suitable for switching DC current.
Was this helpful?
What can we do to improve the information ?