Technical FAQs

Ask a Question

What is the minimum overload setting on the Micrologic 2 trip units?

The NSX Micrologic 2 trip unit overload setting is adjustable between 0.36 and 1 times the rating (In) of the device.
The (Io) front dial on the Micrologic trip units are adjustable between 0.4 and 1 times the rating (In) of the device.
Fine adjustment (Ir=Io x  0.9 to 1 ) may be programmed into the trip unit using the keypad.
Was this helpful?
What can we do to improve the information ?