Technical FAQs

Ask a Question

What is the minimum overload setting on the TM-D thermal magnetic trip units for NS & NSX breakers?

Only the three and four pole devices can be adjusted, single and double devices are fixed.

The NS100 - 250 TM-D thermal magnetic trip units have an adjustment range of between 0.8 - 1 times the rating (In) of the trip unit.

The NSX100 - 250 TM-D thermal magnetic trip units have an adjustment range of between 0.7 and 1 times the rating (In) of the trip unit.
Was this helpful?
What can we do to improve the information ?