Technical FAQs

Ask a Question

Are the iC60H miniature circuit breakers suitable for use on a DC system?

The standard iC60H miniature circuit breakers are suitable for use on DC systems IEC/EN 60947-2.
1 pole 48Vdc 20kA
1 pole 72Vdc 10kA
2 pole 133Vdc 10kA
4 pole 250Vdc 10kA ( in series )

However we also manufacture a specific range of C60-DC ( A9Nxxx ) suitable for use on a DC system which has a higher performance.
1 pole 220Vdc 10kA
2 pole 250Vdc 20kA
2 pole 440Vdc 10kA
2 pole 500Vdc 6kA
Was this helpful?
What can we do to improve the information ?