Technical FAQs

Ask a Question

How do I de-mount the circuit breaker in GenieEvo

The GenieEvo circuit breaker can be de-mounted and replaced in under 1.5 hours.

Full details of how to de-mount the breaker are on the attached procedure.
Was this helpful?
What can we do to improve the information ?