Technical FAQs

Ask a Question

What do I do if the needle is in the red zone on the gas gauge

Do not operate the unit.

Arrange for the unit to be isolated and made safe. Make arrangements for a Schneider Electric engineer to inspect and to investigate why there is low or no gas in the unit.

For more information on low gas in gas filled units please e-mail:
Was this helpful?
What can we do to improve the information ?