Technical FAQs

Ask a Question

Does the Sepam Relay Series 20, 40 and 80 use the same communication protocol as the Digital relay (DR)? (ANSI)

The DR (Sepam 1000 Americanized) communicates with a protocol called PowerLogic (Sy-Max) and the Sepam 20, 40 & 80 uses Mod-Bus RTU , an Industry standard protocol developed by Modicon. These two relays cannot communicate on the same daisy chain. A device such as EGX, ethernet gateway, can interface the two protocols for a common host.
Was this helpful?
What can we do to improve the information ?