Technical FAQs

Ask a Question

Can the Sepam series 80 voltage inputs be connected directly to a 415 V 4-wire 3-phase LV system (without the use of Voltage transformer)

The continuous thermal withstand of the Sepam series 80 voltage inputs is 240V AC, which means that it is not possible to connect the Sepam directly to the network. Furthermore, the Sepam setting tool (SFT2841) does not allow such voltage values to be entered.

 

Was this helpful?
What can we do to improve the information ?