Technical FAQs

Ask a Question

Do the links need to be removed from the NSX current transformer blocks?

The links fitted to the current transformer (CT) blocks are fitted to prevent the CT being damaged if its on-load without a meter being connected.

When the meter is connected to the CT block the links must be removed.


Note:
The links must only be removed if the CT is being connected to a meter, and must not be disconnected if the CT is in a live panel and or if it has any current flowing through it.
Was this helpful?
What can we do to improve the information ?