Technical FAQs

Ask a Question

Can the DIN rail Clips be replaced on miniature circuit breakers. RCD's and other DIN rail devices?

DIN rail clips can be replaced on some of the MCB's, RCD's and other DIN rail devices e.g iC60H MCB's & iID RCD's.

If the DIN rail clips are like the ones in the attached photo the part number is A9A27052 

Note: The DIN rail clips used on the C60H RCBO cannot be replaced.
Was this helpful?
What can we do to improve the information ?