Technical FAQs

Ask a Question

What is the bend radius of uPVC Perimeter Trunking?

Perimeter trunking 40mm ± 2.0mm deep can be bent to a radii of 6.0m minimum, internal or external. Anything smaller, then the trunking has to be segmented (like 20 or 50 pence coin).

Perimeter trunking 50mm ± 2.0mm deep can be bent to a radii of 7.5m minimum, internal or external. Anything smaller, then the trunking has to be segmented.

Perimeter trunking 60mm ± 2.0mm deep can be bent to a radii of 9.0m minimum, internal or external. Anything smaller, then the trunking has to be segmented.

Was this helpful?
What can we do to improve the information ?