Technical FAQs

Ask a Question

Can a Mita pull up tower be used in a kitchen installation?

A TDT pull up tower is not suitable for use in a kitchen environment as it is not sufficiently IP rated and also sockets are only rated 3.15A so would not be suitable for kitchen appliances
Was this helpful?
What can we do to improve the information ?