Technical FAQs

Ask a Question

I require spares for FBX100 floor box are they still available?

Below are the spares for the FBX65, FBX75, FBX100, FBX 120 old floor boxes, parts may be limited due to product being obsolete :
  • 600055 M4 x 8 POZIPAN T/TITE Zinc Plated used to secure the trim
  • 600050 Partition divider
  • 600052 Base Box
  • MFBCAM Cam assembly
  • 600057 M5 x 6 POZIPAN T/TITE Zinc Plated used to secure the partition
  • 6810021 UFB700 lid (grey)
  • FBSCG Cable outlet / Cable flaps (grey)
  • 681055 Lid lifting handle
  • FBSTRIM Trim only
     
Was this helpful?
What can we do to improve the information ?