Technical FAQs

Ask a Question

What is the part number for the Castell lock adapter kit for the NS630b NS800 NS1000 NS1250 and NS1600 extended rotary handles

The part number for the Castell lock adapter kit suitable for the NS630b to 1600 extended rotary handle is NSBCASTELL which is available from Schneider Electric.

The Castell locks used on the extended rotary handle lock kits are only available from Castell.
The Castell lock ordering information is:- 
Castell lock type K form 4
Bolt projection = 19mm
Initial projection = flush
Was this helpful?
What can we do to improve the information ?