Technical FAQs

Ask a Question

What is the part number for the Castell lock used on the NS and NSX extended rotary handle Castell lock kit?

The Castell locks used on the extended rotary handle lock kits 92325 (NSX & NS 100 - 630, NS80H) & NSBCASTELL (NS630b - 1600) are only available from Castell.
The Castell lock ordering information is:-
Castell lock type K form 4
Bolt projection = 19mm
Initial projection = flush
Was this helpful?
What can we do to improve the information ?