Technical FAQs

Ask a Question

What is the part number for the Castell lock used on electrically operated NS630b NS800 NS1000 NS1250?

The Castell locks used on electrically operated NS630B to NS1600 are only available from Castell.
You will need the keylock kit ( without key locks) for Castell kelocks, Part No = 47518 to fit the lock
The lock is part number CL1019
The key is part number CL1062
Was this helpful?
What can we do to improve the information ?