Technical FAQs

Ask a Question

If a circuit breaker is locked in the ON position will it still trip under fault conditions?

All Schneider Electric circuit breakers have a trip-free mechanism, which ensures that the circuit breaker opens under fault conditions even if the operating handle is held in the closed position.
Was this helpful?
What can we do to improve the information ?