Technical FAQs

Ask a Question

Are spare doors and covers available for the Acti9 Isobar Distribution Boards?

Spare doors and covers are available for the current range of Acti9 Isobar Distribution Boards (See below)

Spare doors and covers for older Distribution Boards are not available.

For single phase distribution boards

6 Way - SEA9AN6C
10 Way - SEA9AN10C
14 Way - SEA9AN14C
18 Way - SEA9AN18C
27 Way - SEA9AN27C

For three phase distribution boards

SEA9BN4C 4 way door and cover
SEA9BN6C 6 way door and cover
SEA9BN8C 8 way door and cover
SEA9BN12C 12 way door and cover
SEA9BN16C 16 way door and cover
SEA9BN18C 18 way door and cover
SEA9BN24C 24 way door and cover


 

Was this helpful?
What can we do to improve the information ?