Technical FAQs

Ask a Question

Can the Vigi Residual Current Protection Module be fitted onto the Multi 9 Isobar and Acti 9 Isobar Distribution Board 160A to 250A Incomers?

The add-on Vigi Residual Current Protection Modules cannot be fitted onto the standard 160A to 250A switch disconnector or MCCB incomers.

However, part number  MGNI160RCCB is a switch disconnector with the Vigi Residual Current Protection Module already fitted for Multi 9 Isobar boards or part number SEA9NI160RCCB is a 160A switch with RCD protection for the Acti 9 Isobar board.
Was this helpful?
What can we do to improve the information ?