Technical FAQs

Ask a Question

What is the short circuit rating of the Isobar Distribution Boards?

The single phase Isobar Distribution Board has a fully type tested conditional short circuit rating of 16KA to BS EN 61439-3

The three phase Isobar Distribution Board has a fully type tested conditional short circuit rating of 25KA to BS EN 61439-3 when fed by an MCCB.
Was this helpful?
What can we do to improve the information ?