Technical FAQs

Ask a Question

Can multiple extension boxes be fitted to the three phase Isobar Distribution Boards?

Yes, multiple extension boxes can be fitted to the three phase Isobar and Acti 9 Distribution Boards.

Extension boxes can only be fitted to the IP31 rated boards and not the IP55 heavy duty boards. We would not really recommend more than 2 extesion boxes being stacked.
Was this helpful?
What can we do to improve the information ?