Technical FAQs

Ask a Question

What information is contained in the Sepam series 80 cartridge?

The Sepam series 80 cartridge contains the following information:
  • System and application software (protection functions, protection and parameter settings)
  • Customized monitoring and control functions (matrix, equation editor, customized logic schemes..)
  • Customized working language

This information is saved in the event of a Sepam power failure.
 
Danger: The cartridge must not be removed while Sepam is energized.
Was this helpful?
What can we do to improve the information ?